Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Insights > RF + Microwave
Related Tags
- #Emission Test
- #Calibration
- #Wireless Device Test
- #Design Software
- #4G LTE-A
- #massive MIMO
- #mmWave
- #GNSS
- #Test Automation
- #LTE
- #EMC Pre-Compliance
- #PathWave
- #Design + Automation
- #Signal Studio
- #Arbitrary Waveform Generators
- #Spectrum Analyzers
- #Oscilloscopes
- #6G
- #Signal Analyzers
- #Conducted Test
- #Signal Generators
- #Aerospace + Defense
- #Network Analyzers
- #Software
- #Handheld
- #EW
- #FieldFox
- #Internet of Things
- #Measurement Fundamentals
- #Radiated Test
- #MIMO
- #5G
- © Keysight Technologies 2000–2022
Matt Campbell
RF + Microwave
Consider the Source Part 1: What is a Phase Locked Loop?
2020-12-08 | 5 min read
In this two-part blog we’ll look at how network analyzers generate signals. The phase locked loop is the bread and butter of analog signal generation, and understanding how phase locked loops work is key to understanding network analyzer block diagrams.
What is a phase locked loop and how do they work?
A PLL enables high-frequency signal generation based on a stable, low frequency reference. Figure 1 below shows a general PLL block diagram. A stable, low-frequency reference signal drives a voltage-controlled oscillator (VCO) to output a signal N times the reference frequency. On basic PLLs, N is an integer, but more advanced circuitry enables N to be a noninteger. This type of design is known as fractional-N synthesis.
The frequency divider downconverts the output by a factor of N, and then a phase detector measures the phase difference between the reference signal and the downconverted output. If the frequency of the two signals is the same, then their phase difference is constant. This is where the term “phase locked” comes from – the two signals are locked together with a constant phase difference between them.
Plls in network analyzers
The ability of the PLL to reliably generate high-frequency signals makes it a great candidate for network analyzer signal sources. You can easily sweep across broad frequency ranges by adjusting N. The figure below shows a general network analyzer block diagram with a PLL-based source.
The source generates a test signal that the splitter routes to a reference receiver and the DUT. Measurement receivers sample the transmitted and reflected signals from the DUT. The network analyzer compares the measurements between the reference receivers and the measurement receivers, providing reflected and transmitted signal measurements as relative fractions of the incident test signal.
By sampling the test signal before and after it reaches the device under test (DUT), network analyzers can apply vector error correction for extremely accurate measurements – discontinuities are ratioed out of the measurement. This is important when we consider that the PLL source locks the stimulus and output together by an arbitrary phase difference, meaning your test signal will start at an arbitrary phase. But that’s okay for traditional network analyzer measurements like S-parameters, because the instrument measures the DUT’s response relative to the test signal, not relative to an absolute scale.
That’s enough relatives and absolutes to make your head spin, but the key takeaway is this: phase-locked loops make excellent signal sources for general-purpose network analysis.
However, modern designs containing amplifiers and frequency converters push the limits of what network analyzers can do. For example, when characterizing frequency converters with internal local oscillators, phase noise in the test system and the DUT can contribute to phase errors. If the results include phase errors, it’s impossible to know whether the phase noise came from the network analyzer or the DUT.
Modern mixers and frequency converters also push the limits of a network analyzer’s capabilities. Getting consistent measurements for operating bandwidths as wide as 3.2 GHz at 29 GHz often requires averaging multiple sweeps to reduce the noise.
So what do you do when you’re on the cutting edge of RF and you need to perform advanced network analyzer measurements as efficiently as possible? Find out next week in Part 2, or if you don’t want to wait download the white paper to read about how we upgraded the PNA and PNA-X to make sure they continue to be your go-to as devices continue to go up in frequency and down in size.
Related Content
Consider the Source: Reliable Network Analysis Starts with a Clean Signal
Related Posts
RF + Microwave
VNA Best Captures 5G Amplifier EVM
Gabrielle Duncan 2022.05.12
4 min read
#mmWave #massive MIMO #Network Analyzers #5G
RF + Microwave
Robotic Process Automation Can Optimize Your Test Instrumentation
Andrew Herrera 2022.05.10
9 min read
#Software #Design + Automation #Design Software #Test Automation #PathWave #Oscilloscopes #Signal Generators #Network Analyzers
RF + Microwave
Phase Noise Measurement Matters
Chaimaa Aarab 2022.02.23
6 min read
#Network Analyzers #Measurement Fundamentals