Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Insights > Network Visibility + Security
Related Tags
- #Cloud
- #Packet Brokers
- #Performance Monitoring
- #Cybersecurity
- #Network Security
- #Network Visibility
- #Network Analyzers
- #Data Privacy
- #Software
- #CloudLens
- #Network Taps
- #Test Automation
- #Network Test
- #SDN + NFV
- #Internet of Things
- #Industry Trends
- #Bypass Switches
- #Government
- #Healthcare
- #Data Center Infrastructure
- #Hawkeye
- © Keysight Technologies 2000–2022
Christophe Olivier
Sr. Product Manager – Network Visibility & Virtualization Solutions
Network Visibility + Security
Network Virtualization – Are 3rd party Network Visibility Solutions still relevant?
2020-08-11 | 6 min read
You may or may not be familiar with network virtualization, so let me give a very high-level definition of what it is.
Virtualization started with server virtualization, it allows to run multiple virtual machines (VMs) on the same physical server, each VM being independent from the others. The concept was later expanded to network resources, allowing to reproduce a complete network topology in software. This “software layer” became the foundation of the software-defined data center (SDDC), it brings flexibility unachievable with hardware solutions. With network virtualization, the network administrator can quickly change a network topology by provisioning virtual network components to fit user requirements, this can also be automated for dynamic provisioning. Such flexibility and agility are key to tackle the challenges of cloud environments.
So, with such “smart” networks, are 3rd party Network Visibility Solutions still relevant?
I believe they are, traditional visibility solutions that monitor north south traffic between physical appliances may not be as relevant in a virtual environment where 70+% of the traffic goes east west and does not transits on a physical link. Nonetheless, being able to analyze network packets between VMs or containers is still key for advanced troubleshooting, and this requires visibility solutions specifically designed for virtual environments.
Network virtualization, or Software Defined Networking (SDN) solutions are commercially available, Cisco ACI, Juniper Contrail, Nokia Nuage, VMware NSX, Nutanix to name a few. Some offer network visibility features, but may require specific integration, development, or a complete overhaul of the customer visibility architecture. While that may be acceptable “for green field” fully virtualized deployments, this can be a challenge for customers who want to leverage existing monitoring tool investments, and simply expand their time proven visibility solution to their virtual environment. Another important point is trust, can you trust the entity which is managing your infrastructure to tell you that everything is running fine and secure? I heard that concern several times, getting an external view may not be a bad idea.
It is where CloudLens, Keysight visibility solution for virtualized environment becomes the link between the SDN and the global visibility solution.
VMware already occupies a significant market share in enterprise SDDC, and VMware NSX, is a natural choice as their SDN. That’s why Keysight partnered with VMware to expand its CloudLens network visibility solution to offer the integration with NSX, first with NSX for vSphere (NSX-V) and the latest edition for NSX Data Center, previously known as NSX-T. If you need complete, packet-level visibility, CloudLens virtual taps (vTap) will bring additional packet filtering capabilities, metadata (NetFlow) generation and integration with Keysight global network visibility solution for additional packet processing, deep packet inspection, application identification and filtering, threat detection…Allowing customers ensure that their SDDC is fully covered by their visibility solution.
How it works
VMware NSX Data Center is a full virtualized networking and security solution which offers network introspection capabilities. And CloudLens includes a specific integration of its virtual tap (vTap) with this network introspection functionality; to capture and filter network packets and even generate metadata, for individual service chains. This provides additional flexibility when network resource optimization is important.
CloudLens leverages NSX service chain mechanism to insert the CloudLens as a network introspection service, the service then integrates with NSX Security Groups and Policies to become part of the NSX architecture. To simplify the administrator’s tasks, the deployment lifecycle is managed from the NSX Manager. The network administrator can choose between deploying CloudLens virtual taps service virtual machine (SVM), per host or per cluster of hosts.
The NetX API and “Copy Packet” features mirror the East/West traffic of select VMs to CloudLens vTap (traffic capture is based on NSX Security Groups and Policies). CloudLens vTap can then process the received mirrored traffic, apply additional filtering
The representation below gives an overview of how the CloudLens solution provides network visibility of east-west traffic in a VMware NSX Data Center environment.
Highlights
CloudLens, Keysight visibility solution for virtualized environments:
CloudLens also provides network visibility for VMs and containers in multiple virtual environments, VMware, Kubernetes, Microsoft Hyper-V, Nutanix, OpenStack KVM. For more information please see the CloudLens page on the Keysight website, for more info about the integration with Nutanix AHV, see this blog post.
Related Posts
Network Visibility + Security
Cyber Resilience – The Most Important Asset for Healthcare
Keith Bromley 2022.06.30
3 min read
#Healthcare #Network Visibility #Network Security #Cybersecurity
Network Visibility + Security
3 Steps to Securing Your Healthcare Network
Keith Bromley 2022.06.16
5 min read
#Healthcare #Network Security #Network Visibility
Network Visibility + Security
RSA 2022 Is A Wrap
Keith Bromley 2022.06.14
4 min read
#Network Security #Network Visibility