Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Insights > Benchtop
Related Tags
- #PAM4
- #Calibration
- #BenchVue
- #Wireless Device Test
- #Design Software
- #Thermal Profiling
- #Energy Ecosystem
- #Test Automation
- #BERT
- #PathWave
- #Design + Automation
- #Autonomous Driving
- #Digital Multimeters
- #Arbitrary Waveform Generators
- #Data Center Infrastructure
- #Spectrum Analyzers
- #DDR5
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Oscilloscopes
- #Data Acquisition
- #Automotive Ethernet
- #Power Supplies
- #Digital Signal Processing
- #Signal Analyzers
- #PCIe
- #Oscilloscope Apps
- #Ethernet
- #Aerospace + Defense
- #PCIe 5.0
- #products
- #Software
- #400GE
- #In-Circuit Test Systems
- #Internet of Things
- #DDR4
- #5G
- © Keysight Technologies 2000–2023
Kwan Wee Lee
Technical Marketing Engineer
Benchtop
Reduced development time with PathWave Test Executive for Manufacturing
2022-10-31 | 6 min read
Have you heard about the new PathWave Test Executive for Manufacturing(PTEM)?
It’s an open-source solution packed with user-friendly interfaces and built-in test steps. If you are familiar with our Test Executive SL, then PTEM is no stranger as it supports the same TS5000 instrumentation libraries as Test Executive SL. On top of that, built on Open Tap open-sourced platform, you can develop your own plug-ins of test steps and libraries. And if that is not enough, just assign any .NET-based Dynamic Link libraries(DLL) to your testplan and you are good to go.
Let me share my experiences as a first-time user of PTEM in developing a testplan for the FlexiCore Inline parallel ICT system.
Over 200 instrumentation libraries are built into PTEM along with their test steps functions. You simply choose the instruments you need and pick the test step to use in the testplan. That’s all it is. No need for code development at all.
PTEM also supports common protocols like LAN and Serial ports which can be used with generic instruments or systems. In my earlier posts about test automation control, I discussed the SCPI commands to control the FlexiCore Inline parallel ICT handler over LAN interface. The same set commands can be applied in a PTEM testplan as well.
Assigning SCPI instrument
Testplan development starts with the selection a generic SCPI instrument and assigning the address for the Handler Control Panel (HCP) application that manages the handler operation. PTEM automatically lists all addresses from Keysight IO Library Suite, so all you need to do is to select the one you need.
The Virtual Instrument Software Architecture (VISA) address for HCP to configure in the IO Library is IP address 127.0.0.1 with socket 5045 when PTEM resides in the same PC controller as HCP. PTEM can also run remotely from another PC controller within the same network. In that case, the IP address for HCP application will need to be the actual IP address of the network adaptor instead of using 127.0.0.1. The VISA address will then look something like this “TCPIP::192.168.0.20::5045::SOCKET”, where 192.168.0.20 is the IP address of the network adaptor.
Commands for test operation
A basic test operation cycle on the FlexiCore consists of four stages: Initialization , Input, Test and Output stage. It only takes four commands to get the test operations running. My post on “Controlling Test Automation - The Easy Way” provides the details of the control sequence.
The commands are not specifically built into PTEM. However, it is not difficult to use the SCPI Ext test step to execute them. SCPI Ext is a generic test step that allows me to control any instruments that supports TCPIP socket protocol.
Testing the setup
While you can dive right into the commands and control of the handler after the test steps are setup, I prefer to test each of the instruments first before proceeding further. This gives me the confidence that the instruments and test steps parameters are set up correctly.
The HCP supports the command *IDN? which returns an identification string showing the version of the application. This is very useful when it comes to checking whether the TCPIP link to the application is still active or not.
The testplan above sends the *IDN? command to HCP and then places the received response into a variable named VAR.ID1. Using variables to store measurements and return strings from instruments or logical/arithmetic results are essential in the testplan development. The Watch Variables Panel under the View menu displays the status of selected variables in real time throughout the execution of the testplan. This allows me to monitor the results from any test steps easily during the testplan development.
Now that I got the basic instrument and command setup in my testplan, I can start to build the flow of the test steps to run the handler operations. I will share more on PTEM as I continue to explore the features and functions.
Until the next post, stay healthy and safe!
Ping me with your questions or comments !
kwan-wee_lee@keysight.com
Related Content
Products
PathWave Test Executive for Manufacturing
Keysight FlexiCore Automated Inline Parallel In-Circuit Test System
Related posts
Controlling Test Automation - The Easy Way
Test Automation in your hands
Related posts
Automate Your Functional Test
Are you ready for parallelism test?
Related Posts
Simulation + Design
The World of Possible What-Ifs: Exploring the Limitless Potential for Digital Twin Technology
Jenn Mullen 2023.01.27
10 min read
#Industry Trends #Network Security #Design + Automation #STEM
Benchtop
Sharing variables between test projects
Kwan Wee Lee 2022.12.31
6 min read
#Automotive + Energy #Automotive Ethernet #Autonomous Driving #Test Automation #Design + Automation #Manufacturing Test #In-Circuit Test Systems #PathWave
Benchtop
How to pick the optimal power solution for satellite solar array testing
Brian Whitaker 2022.12.05
6 min read
#Power Supplies #Manufacturing Test #Aerospace + Defense