Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Insights > Benchtop
Related Tags
- #PAM4
- #Calibration
- #BenchVue
- #Wireless Device Test
- #Design Software
- #Thermal Profiling
- #Energy Ecosystem
- #Test Automation
- #BERT
- #PathWave
- #Inclusion + Diversity
- #Design + Automation
- #Autonomous Driving
- #Digital Multimeters
- #Arbitrary Waveform Generators
- #Data Center Infrastructure
- #solutions
- #Spectrum Analyzers
- #DDR5
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Oscilloscopes
- #Data Acquisition
- #Automotive Ethernet
- #Power Supplies
- #Digital Signal Processing
- #Signal Analyzers
- #PCIe
- #Oscilloscope Apps
- #Ethernet
- #Aerospace + Defense
- #Education
- #PCIe 5.0
- #Network Analyzers
- #products
- #Software
- #400GE
- #In-Circuit Test Systems
- #Internet of Things
- #DDR4
- #5G
- © Keysight Technologies 2000–2023
Kirk Jensen
Benchtop
PCIe® 6.0: The Next Evolution of PCIe
2022-04-21 | 3 min read
Background
Peripheral Component Interconnect Express (PCIe®) is a core technology that many types of computer servers and endpoint devices use. Advances in this technology allow users to drive innovation in 5G, cloud computing, hyperscale data centers, and beyond. The PCI Special Interest Group (PCI-SIG®) defines specifications and compliance tests that guarantee the interoperability of PCIe systems. Evolving from PCIe® 1.0 in 2003 and supporting 2.5 gigatransfers per second (GT/s), the current PCIe standard, PCIe 6.0, came out in 2022 and supports 64 GT/s.
A Significant Upgrade
PCIe 6.0 technology is the first PCI Express® standard to use pulse amplitude modulation 4-level (PAM4) signal encoding, enabling PCIe 6.0 devices to achieve twice the throughput of PCIe 5.0 devices while maintaining the same channel bandwidth, low power, and backward compatibility with previous generations. The PCIe 6.0 standard uses the same high-level approach for transmitter (Tx) and receiver (Rx) testing while adding new transmitter measurements that are specific to PAM4 encoding. Like previous generations, PCIe 6.0 devices employ Tx and Rx equalization along with requiring forward error correction (FEC). Because FEC causes a latency increase, PCIe 6.0 introduces flow control unit (FLIT) encoding. PCIe FLITs eliminate the need for extra packet overhead, thus reducing overall latency by offsetting the increase from FEC.
Compliance Testing
The PCI-SIG requires vendors to conduct compliance testing for interoperability that includes a list of preset or transmitter equalization settings which must be electronically verified. You must conduct three categories of testing to reach official PCI-SIG approved compliance: the physical layer, the data link layer, and general interoperability. When reviewing the standard, you will notice that the PCIe specification framework consists of multiple specifications: Base, Card Electromechanical (CEM), and Test. These specifications define what you need to understand, and test, to comply with the PCIe standard.
Test Solutions
Regardless of which generation of the PCIe specification you are working on, you need a test solution the PCI-SIG aligns with to ensure that your products comply with the standard and get to market faster. Keysight provides a total-solution approach to test all generations of the PCIe specifications so you can focus on your next design, rather than spending time learning the details of the test procedures and requirements.
For more information, read the white paper: The Evolution of PCIe® Standards and Test Requirements
Related Content
PCIe Receiver Testing Solutions
N5991PB6A PCIe 6.0 Base Specification Receiver Test Automation
M8000 Series Bit Error Ratio Testers (BERT)
PCIe Transmitter Testing Solutions
SW02PCIE PCI Express Full Tx Test Suite
UXR-Series Oscilloscopes
PCIe Design and Simulation Solutions
W3625B PathWave ADS Core + EM Design + Layout + HSD Ckt Sim + SIPro + PIPro
W3082E PathWave PCIe AMI Model Builder
Related Posts
Industries
Digital Twins: Is it real or is it EDA?
Albert Lee 2023.03.29
7 min read
#Design + Automation #Design Software #Oscilloscopes #Signal Analyzers
Benchtop
USB 80Gbps: What's New in USB4 Version 2?
Ben Miller 2022.11.08
7 min read
#Oscilloscope Apps #Data Center Infrastructure #Design Software
Industries
ECOC 2022 Discoveries
Stephanie Michel 2022.10.03
3 min read
#Optical + Photonic #Data Center Infrastructure #800G #Arbitrary Waveform Generators #BERT