Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Insights > Benchtop
Related Tags
- #PAM4
- #Calibration
- #BenchVue
- #Wireless Device Test
- #Thermal Profiling
- #Energy Ecosystem
- #Test Automation
- #BERT
- #PathWave
- #Design + Automation
- #Digital Multimeters
- #Arbitrary Waveform Generators
- #Data Center Infrastructure
- #Spectrum Analyzers
- #DDR5
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Oscilloscopes
- #Data Acquisition
- #Power Supplies
- #Digital Signal Processing
- #Signal Analyzers
- #PCIe
- #Oscilloscope Apps
- #Ethernet
- #Aerospace + Defense
- #PCIe 5.0
- #Software
- #400GE
- #Internet of Things
- #DDR4
- #5G
- © Keysight Technologies 2000–2022
Bernard Ang
Product Marketing
Benchtop
Monitor Battery Temperature By Using a Data Acquisition System or Specialized Battery Test System
2021-12-02 | 8 min read
In today’s electronics applications, batteries power nearly all of our portable electronic devices. Batteries also serve as emergency power backup systems on large premises. All-electric vehicles use large cascading battery packs to meet the expected power for the required performance. Battery packs need the required specific power (W/kg) to be able to dispense enough current to achieve the electric vehicle speed performance. They also need the required specific energy (Wh/kg) to achieve longer runtime or travel range.
Why is it important to monitor battery temperature?
Most rechargeable batteries today use lithium ion and have an operating range between 15 °C and 35 °C at which their full performance and capacity kicks in.
The power map chart below shows the power limits of your lithium-ion battery cell, module, or packs across the temperature range. The range between 15 °C and 35 °C is the optimum operating temperature range for the batteries to achieve full performance. The temperature range is also the most efficient, reliable, and safe range for battery operation.
When to use a data acquisition (DAQ) system for monitoring battery temperature
A data acquisition (DAQ) system is one of the most versatile instruments to measure the temperature of physical objects or multiple objects. A DAQ system monitors temperature at multiple points in a product’s battery system. Typically, you initially test functional design blocks independently, and then you test sub-integrated design blocks during a product design and development stage. Testing for lab battery packs and systems occurs during an early product design cycle using several common R&D lab instruments.
A DAQ system can be used to monitor temperature at multiple points in a product’s battery system. Charge the battery system with a DC power supply and use a DC electronic load to discharge the battery system. Figure 2 below shows a common lab setup using a DAQ system.
If you happen to own a bidirectional DC power supply that can source and sink current, then you can replace the separate DC power supply and DC electronic load with a bidirectional DC power supply.
Using Keysight’s PathWave BenchVue software application, you can quickly set up and execute tests and get results faster. The application’s test flow feature allows you to build automated tests and reduces test development time significantly. The test flow feature also enables the simple sequencing of instrument settings and measurements, and combines multiple instruments to help you create your own automated test.
PathWave BenchVue software allows you to:
When to use a specialized battery test system for monitoring battery temperature
Performing quick workarounds on bench test instruments may serve you well for quick troubleshooting and verifying your battery system design. However, when you need a dedicated and well-supported specialized battery test system, Keysight’s Scienlab battery test systems provide reliable and precise testing of battery systems whether they are in the cell, module, or at the pack level. Figure 3 below shows how Keysight Scienlab battery test systems are scalable from individual stand-alone solutions, to fully integrated test systems and ready-to-use test laboratories.
The Scienlab SL1000A series battery pack test system for example, is scalable up to 1000 V, ± 2400 A, and ± 360 kW. The battery test system is suitable for various energy storage applications ranging from automobile transportation, to industrial and other large on-premise use cases.
The Keysight Scienlab SL100XA series battery test system offers many features that make it a standout in the market. The system comes with integrated test environments for your device under test (DUT) such as temperature and climate chambers, conditioning for your DUT, and standardized contacting systems and integration to your DUT. There are also built-in safety and security mechanisms to help you avoid potentially hazardous situations.
Summary
Monitoring battery temperature occurs throughout the battery system’s product life cycle. During the early stages of the product life cycle, engineers can quickly troubleshoot and validate their battery system designs with bench instruments such as a DAQ, in conjunction with a current sourcing and sinking DC power supply. During the characterization and qualification stages of the product life cycles, the Keysight Scienlab battery test solution becomes invaluable to help you ensure a precise and volume scalable test solution.
Ultimately, the purchase decision depends on your test applications, budget, and specifications. To learn more about the DAQ system for temperature measurements, visit https://www.keysight.com/us/en/products/modular/data-acquisition-daq.html, and to learn more about DC power supplies, visit https://www.keysight.com/us/en/products/dc-power-supplies.html.
For more information on the Keysight Scienlab battery test system, visit https://www.keysight.com/us/en/products/hev-ev-grid-emulators-and-test-systems/scienlab-battery-test-systems.html.
Related Posts
Benchtop
What is Power Integrity and How Do I Measure It?
Ben Miller 2022.08.02
10 min read
#Oscilloscope Apps #Power Supplies #Oscilloscopes
Insights
IC Wire Bond Deformation Detection
Kwan Wee Lee 2022.06.27
5 min read
#Semiconductor #Automotive + Energy #Automotive Ethernet #Autonomous Driving #In-Circuit Test Systems #Manufacturing Test
Insights
Detecting Near Short Defects in IC Wire Bonds with VTEP Technology
Kwan Wee Lee 2022.06.01
6 min read
#Automotive + Energy #Automotive Ethernet #Autonomous Driving #Manufacturing Test #In-Circuit Test Systems #Design + Automation #Test Automation #Semiconductor #Industry Trends