Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Insights > Benchtop
Related Tags
- #PAM4
- #Calibration
- #BenchVue
- #Wireless Device Test
- #Thermal Profiling
- #Energy Ecosystem
- #Test Automation
- #BERT
- #PathWave
- #Design + Automation
- #Digital Multimeters
- #Arbitrary Waveform Generators
- #Data Center Infrastructure
- #Spectrum Analyzers
- #DDR5
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Oscilloscopes
- #Data Acquisition
- #Power Supplies
- #Digital Signal Processing
- #Signal Analyzers
- #PCIe
- #Oscilloscope Apps
- #Ethernet
- #Aerospace + Defense
- #PCIe 5.0
- #Software
- #400GE
- #Internet of Things
- #DDR4
- #5G
- © Keysight Technologies 2000–2022
Erin East
Benchtop
New 1000 X-Series Oscilloscopes and the Return of Wave Giveaway!
2019-01-08 | 8 min read
Today is a very exciting day! Not only are we announcing two new 1000 X-Series oscilloscopes, but I am also happy to say that Wave is back for 2019.
We will be giving away some of the new oscilloscopes (along with other bench test gear) during the Wave 2019 online event from March 1 through March 15. You can find more details about Wave and the other instruments we will be giving away toward the end of this blog, but first things first: the new 1000 X-Series models.
Check out how-to tips and tricks for the new 1000 X-Series.
The new 4-channel, 200 MHz InfiniiVision 1000 X-Series models help you get measurements you can count on so you can create designs that will change the future. The DSOX1204A and DSOX1204G oscilloscopes leverage the same, proven technology we use in our higher-end InfiniiVision family, giving you professional-level measurements you can trust. Now you can get even more functionality from the 1000 X-Series with capabilities like 4-wire SPI decode and remote connection via LAN.
“Entry level” does not have to mean poor quality and performance. Just because you are on a budget, you shouldn’t have to settle for lesser technology. With industry-leading software analysis and high-end hardware technology, you can measure with a high degree of accuracy at an affordable price. The advanced capabilities like fast Fourier transforms, mask testing, and segmented memory, help quickly analyze and determine signal parameters.
You can have confidence in your measurements knowing you are testing on Keysight-custom technology. The MegaZoom IV ASIC allows for a consistent 50,000 waveforms/second update rate and the highest-sample rate in this class at 2 GSa/s. This means you have a higher chance of catching rare glitches or errors that might not be seen on a similarly priced instrument from another oscilloscope vendor.
The 6-in-1 instrument integration in the 1000 X-Series lets you test more efficiently with twice as many built-in instruments compared to the other entry-level options out there. Not only are you getting all the benefits of a high-quality oscilloscope, you’ll also have:
Upgrading your 1000 X-Series oscilloscope is easy. You can enable the serial decoding options and install bandwidth upgrades at any time by purchasing the software license key. These two new models (DSOX1204A and DSOX1204G) can be upgraded from 70 MHz of bandwidth to 100 MHz or 200 MHz. This way you can purchase the bandwidth you need now, and upgrade as your designs evolve in the future.
Learn how to use the advanced capabilities faster with a simple, intuitive user-interface and access to built-in help and training signals:
And lastly, the standard LAN connectivity lets multiple engineers work on one instrument by connecting to the network via LAN and accessing an internet browser for remote control. This allows students and coworkers to share equipment and work on projects from anywhere, saving time and money.
With all of this, you can measure with confidence and dedicate more time and money to your designs rather than your test gear.
WAVE 2019
For limited time, you have a chance to win one of these new oscilloscopes!
During Wave 2019, not only will we be giving away the new 1000 X-Series oscilloscopes, but we will also be drawing names to win some of the higher-end touch screen oscilloscopes, power supplies, benchtop and handheld multimeters, waveform generators, and more. We’re giving away over 100 instruments this year, so this gives you even more chances to win than last year. That’s over $375,000 worth of prizes!
Every weekday March 1 - March 15, we will be drawing winners for prizes, and of course we will be returning with more measurement tips so you can learn how to better use all of these instruments. You can enter the giveaway drawing once per day March 1 through March 15, but starting January 8, 2019, you can register for one early entry as well.
The daily entries continue to build on top of each other. You do not have to enter every day to be eligible to win that day’s drawing. Say that you only enter your name today. Well, your name will still be in the bucket of names that we draw from until the end of the event on March 15. You can enter by going to http://www.wavekeysight.com/.
However, Wave isn’t only about the giveaway. It’s also about empowering you to perform even better tests. Once you register for Wave 2019, on March 1 you will gain access to content designed to help you understand how to measure and analyze your signals more effectively.
Keeping up with tradition, we will be kicking everything off with another live stream on March 1. Be sure to add that date to your calendar so you can come back and see if you’re one of our first winners, and what else is in store for Wave 2019.
Related Posts
Benchtop
Two Domains Are Better Than One: Oscilloscopes and Signal Analyzers
Rick Clark 2022.08.04
10 min read
#Oscilloscope Apps #Signal Analyzers #Spectrum Analyzers #Oscilloscopes #Wireless Device Test
Benchtop
What is Power Integrity and How Do I Measure It?
Ben Miller 2022.08.02
10 min read
#Oscilloscope Apps #Power Supplies #Oscilloscopes
Simulation + Design
How to Automate Ethernet Testing
Andrew Herrera 2022.07.25
3 min read
#PathWave #Test Automation #Design + Automation #Ethernet #Oscilloscopes #Software