Testing the Hearts of Electric & Hybrid Vehicles

A good idea is never lost, as Thomas Edison said. At the turn of the 20th century, nearly 30% of all cars manufactured in the US were electric-powered, but by the 1920s they had effectively disappeared, thanks to cheap gas and mass production of conventional cars. But fast-forward 100 years and electric cars are back with a vengeance, in response to rising fuel prices and Government-mandated emissions controls.

The number of pure electric and plug-in hybrid cars on the world’s roads passed the 3-million mark in 2017, and will accelerate to over 5 million by the end of 2018, according to analyst EV-Volumes. This rapid growth in production volumes is being matched by equally rapid advances in powertrains, power electronics and battery technologies.

These advances also highlight the increasingly critical role played by a previously unsung vehicle component:* the DC:DC converter*. Irrespective of whether a car is a pure EV or a hybrid, DC/DC voltage conversion is at the heart of its power electronics systems. It manages the energy exchange between the vehicle’s high-voltage (HV) bus which serves the main HV battery, electric traction which drives the motors and generators, and the traditional 12 V power bus, from which most of the car’s electrical systems (in-car entertainment, navigation, heating, lights and more) are powered.

The converter is fundamental to the overall efficiency and performance of electric vehicle (EV) and hybrid vehicles, for several reasons:

Given the pace of development of vehicles, and the constant pressure to keep costs down across the test and development lifecycle for converters, efficient simulation, design, validation, and manufacturing test of the converters is essential. But this, in turn, presents its own challenges

Converter testing challenges

The design and test obstacles result from many factors:

Converting challenges into solutions

To address these design and test issues, Keysight has developed and introduced new, innovative approaches that help manufacturers accelerate their programs. For example, high-frequency enabled simulators can accurately simulate the behavior of new WBG semiconductors, helping to improve the efficiency of DC:DC converter designs.

New, fully integrated source/sink solutions enable more accurate simulation and testing of DC:DC converters’ transitions in power flow direction during acceleration and regeneration. These test solutions also feature the ability to return clean power to the test lab’s AC mains, reducing regenerative heat and dramatically cutting the need for costly HVAC equipment in the test system environment.

Find out more about how Keysight enables more accurate and efficient testing of the systems at the heart of the electric and hybrid vehicle revolution here.

limit
3