Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Industry Insights
Related Tags
- #Critical Communications
- #Customer Privacy
- #Wireless Device Test
- #Public Safety
- #Network Visibility
- #Energy Ecosystem
- #Test as a Service
- #BERT
- #PathWave
- #Network Test
- #Design + Automation
- #Communications
- #Autonomous Driving
- #SDN + NFV
- #Optical + Photonic
- #Lightwave Component Analyzers
- #Services
- #Arbitrary Waveform Generators
- #DDR5
- #GDPR
- #Oscilloscopes
- #Network Security
- #Data Analytics
- #PCIe
- #Education
- #PCIe 5.0
- #STEM
- #Software
- #Environmental Sustainability
- #Semiconductor
- #Industry Trends
- #KeysightCare
- #Healthcare
- #PAM4
- #Calibration
- #Cybersecurity
- #massive MIMO
- #Data Privacy
- #Design Software
- #mmWave
- #EMC Pre-Compliance
- #Data Center Infrastructure
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Automotive Ethernet
- #6G
- #Connected Car
- #Aerospace + Defense
- #Tunable Laser Sources
- #Gen 5
- #Network Analyzers
- #400GE
- #Sustainability
- #Signal Monitoring
- #In-Circuit Test Systems
- #EW
- #Internet of Things
- #Consulting Services
- #MilCom
- #Radiated Test
- #MIMO
- #5G
- #Blockchain
- © Keysight Technologies 2000–2021
- Privacy
- Terms
- Feedback
- Contact Us
Nicole Faubert
Industry Solutions Director
Industry Insights
What is DDR5?
2020-04-30 | 6 min read
Each new generation of the DDR synchronous dynamic random access memory (SDRAM) standard delivers significant improvements over the previous generation including increased speeds, reduced footprint, and improved power efficiency. However, these improvements introduce new design and test challenges for chip designers and device manufacturers.
The DDR5 standard, defined by the Joint Electronic Devices Engineering Council (JEDEC) organization, will operate at data rates up to 6.0 gigatransfers per second (GT/s) or higher. DDR5 effectively doubles the data rate of DDR4, which supports speeds up to 3.2 GT/s.
The Benefits of DDR5
With IoT enabling billions of internet-connected devices, data center operators must find ways to meet ever-increasing data and storage demands, while preserving the quality of service and minimizing costs. Power is a premium resource for data center operators and minimizing power consumption is one of their top priorities to reduce operating expenses. Each new generation of DDR SDRAM provides increased data transfer speeds, with more memory in a smaller package size that uses less power. Since power reduction is a critical requirement in mobile devices as well — due to the size and weight constraints of batteries — the JEDEC also introduced a low-power DDR (LPDDR) standard. As the name implies, the LPDDR standard uses lower signal amplitude, reducing power consumption.
DDR5 Introduces New Design and Test Challenges
As the speed of DDR technology increases, engineers face new design and validation challenges. Design error margins decrease, and signal integrity becomes more challenging to maintain. Test and measurement solutions enable DDR5 designers to optimize their transmitter, receiver, and channel designs for best performance and reliability at the increased data transfer rate of 6 GT/s.
DDR Design and Simulation
Each new version of the DDR standard supports faster access to data stored in memory. Design and simulation of next-generation DDR5 memory designs enable chip designers and device manufacturers to discover issues before silicon tapeout and to maximize the signal integrity of their designs. Using design and simulation tools, DDR5 designers can quickly resolve signal integrity issues, ensure power efficiency, and stay within tight error margins before first prototypes.
DDR Physical Layer Test
DDR5 transmitter (Tx) and receiver (Rx) designs need to comply with the DDR specifications defined by the JEDEC to ensure interoperability with components and devices from other vendors in the system. Each new generation of the standard introduces new DDR physical layer test requirements. DDR5 introduces new receiver compliance tests, not required in previous generations of the standard. Measurement methods and tools developed to test to precise industry specifications allow designers to focus on designing instead of trying to understand the details and requirements of each new generation of the standard. The right test solutions ensure the quality and performance of next-generation DDR designs and help companies get them to market faster.
DDR Protocol Validation
Data corruption is a common symptom encountered during validation of DDR designs, and its root cause can be difficult to determine. Usually, there are either signal integrity or functional issues with the designs. When DDR memory systems do not behave as expected, designers need functional debug, analysis, and protocol compliance validation solutions. Test solutions that provide trace capture and analysis capabilities provide designers the insight required to understand their system’s behavior and quickly find the root cause of any issues.
DDR memory is everywhere — not just in servers, workstations, and desktops, but also embedded in consumer electronics, automobiles, and other system designs. The DDR standard provides fast access to data stored in memory in a multitude of consumer devices, as well as in the data center. DDR5, the latest development of the standard, will provide double the bandwidth and memory capacity of DDR4. With data transfer rates up to 6 GT/s and 1 Tb of memory, DDR5 will be able to support 400GE speeds in the data center. Selecting test tools that thoroughly test to DDR5 specifications for design and simulation, characterization, and validation will ensure the performance and interoperability of next-generation DDR5 devices.
To learn more about test solutions to simulate, characterize, and validate your DDR designs, check out the DDR Design and Test Solution web page.
Related Posts
Technical Insights
Relief on the Search of Burst Errors
Stephanie Michel 2021.01.19
5 min read
#Data Center Infrastructure
Network Visibility + Security
Data Center Visibility – Go Big or Stay Blind
Jason Lackey 2020.12.04
3 min read
#Network Visibility #Data Center Infrastructure
Industry Insights
Reduce Test Time from Hours to Minutes
Nicole Faubert 2020.07.31
3 min read
#Data Center Infrastructure #400GE