Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Industry Insights
Related Tags
- #Critical Communications
- #Customer Privacy
- #Wireless Device Test
- #Public Safety
- #Network Visibility
- #Energy Ecosystem
- #Test as a Service
- #BERT
- #PathWave
- #Network Test
- #Design + Automation
- #Communications
- #Autonomous Driving
- #SDN + NFV
- #Optical + Photonic
- #Lightwave Component Analyzers
- #Services
- #Arbitrary Waveform Generators
- #DDR5
- #GDPR
- #Oscilloscopes
- #Network Security
- #PCIe
- #Data Analytics
- #Education
- #PCIe 5.0
- #STEM
- #Environmental Sustainability
- #Semiconductor
- #KeysightCare
- #Healthcare
- #PAM4
- #Calibration
- #Cybersecurity
- #massive MIMO
- #Data Privacy
- #Design Software
- #mmWave
- #EMC Pre-Compliance
- #Data Center Infrastructure
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Automotive Ethernet
- #6G
- #Connected Car
- #Aerospace + Defense
- #Tunable Laser Sources
- #Gen 5
- #Network Analyzers
- #400GE
- #Sustainability
- #Signal Monitoring
- #In-Circuit Test Systems
- #EW
- #Internet of Things
- #Consulting Services
- #MilCom
- #Radiated Test
- #MIMO
- #5G
- #Blockchain
- © Keysight Technologies 2000–2021
- Privacy
- Terms
- Feedback
- Contact Us
Stephanie Michel
Technical Marketing Engineer
Industry Insights
Relief From the Worst 400GE Measurement Pains
2019-09-24 | 4 min read
The move from NRZ-based 100G interfaces to PAM4-based 400GE interfaces is revolutionary, rather than evolutionary: New technologies such as linear broadband amplifiers and drivers as well as adaptive digital equalizers have become a mandatory part of the design but are not sufficient to ensure error-free operation. 400GE links typically operate at rather high intrinsic bit error rates (BER) and forward error correction (FEC) is therefore required.
The combination of adaptive equalization and FEC has drastically increased the level of complexity in the characterization and validation of silicon devices, application-specific integrated circuits (ASICs), fiber and copper interconnects, optical transceivers, and the port electronics of switches and routers. Identifying potential performance and interoperability issues at an early stage is critical as answers are complex and time-consuming to solve.
The main challenge to test 400GAUI-8 interfaces here is until now to generate the prescribed stress on the lane under test, while providing the correct unstressed data patterns on the adjacent seven data lines requires to support the striped FEC required by the host FEC decoder on the host chip. For 400G optical transceiver module designers it has been a pain to verify the frame loss ratio (FLR) within the specified limits.
Keysight is now introducing the N4891A / 400GE-QDD, the industry’s first 400GE FEC aware RX test solution, causing ample relief.
The solution combines the versatile and accurate M8040A 64 Gbaud high-performance BERT to provide the stressed pattern to the lane under test, along with the A400G-QDD 400GE multiport module tester from Ixia to produce the striped pattern on the adjacent aggressor lanes, with the perfect synchronization, and allows bit error ratio (BER) and FLR measurements.
High signal integrity RF components allow to take full advantage of the 400GE multiport module tester four QSFP-DD ports, enabling R&D & validation engineers to support a large variety of test setups: such as electrical or optical receiver tests for components or optical transceiver modules.
It empowers the industry to accelerate the deployment of next generation 400GE devices in the datacenters. It provides unique insights to understand how component and system design tradeoffs are affected by Forward Error Correction (FEC) requirements and to predict the system margin under real conditions. This solution allows measurement of frame loss ratio in 400G Ethernet links using FEC by supplying one stressed lane, while maintaining the proper FEC striped test pattern data, without stress on the other lanes.
Find out more.
Related Content
Solutions
Data Center Transceiver Test
Pulse Amplitude Modulation (PAM)
Related Products
M8040A 64 Gbaud High-performance BERT
M8070B System Software for M8000 Series of BER Test Solutions
Resources
White Paper - 400G and Beyond in the Data Center
Webinar - Addressing 400G FEC Challenges on Your Devices
Related Posts
Technical Insights
Relief on the Search of Burst Errors
Stephanie Michel 2021.01.19
5 min read
#Data Center Infrastructure
Network Visibility + Security
Data Center Visibility – Go Big or Stay Blind
Jason Lackey 2020.12.04
3 min read
#Network Visibility #Data Center Infrastructure
Industry Insights
Reduce Test Time from Hours to Minutes
Nicole Faubert 2020.07.31
3 min read
#Data Center Infrastructure #400GE