Testing Active Cables at 112 Gbps Signaling Rate

Active Cables for Networking

Efficient sharing of computing and storage resources is critical for data centers and high-performance computing clusters. For this purpose, specialized servers are linked to each other via switches. The first level of connection takes place in the server rack, where servers are interconnected via a top of the rack (TOR) switch using passive and/or active cables. Layer 1 and Layer 2 switches (also called leaf and spine switches) are used to share resources between racks. As they are usually more than 5 meters away from each other, more expensive and power-consuming optical transceiver modules are used for the connections (see Figure 1).

Figure 1: Data center switching architecture

When passive direct-attached copper (DAC) cables are used, the “host” chip of the networking interfaces sitting at each end of the DAC must accommodate for the loss and distortion of the passive copper channel. This sets very stringent requirements on the host chip design and drastically limits the cable reach when operating at 50 Gpbs or 100 Gpbs signaling rates. For this reason, active cables are becoming increasingly popular.
Due to the varying reach objectives, there are several different types of active cables: active copper cables (ACC), active electrical cables (AEC), and active optical cables (AOC).

Figure 2: Application space for DAC, AEC and AOC according to the Hiwire consortium

A simple linear amplifier and an analog equalizer are typically used in ACCs, whereas AECs and AOCs include a retimer chip that considerably relaxes requirements on the host chip compared to DAC-cable-based on-clock recovery (CR). The so-called chip-to-module (C2M) interface is identical to the one of optical transceiver modules. Contrary to classical pluggable optical transceivers, there is no need to test the optical client “side”, the link between the two ends of the cable being a cable vendor implementation, only the interface to the host (chip-to-module interface).

OSFP Switch

Figure 3: OSFP switch capable of supporting AEC (purple) or DAC (black) cables.

Both the IBTA (InfiniBand Trade Association) and IEEE (Institute of Electrical and Electronics Engineers) Standards Association provides compliance test procedures to ensure interoperability between active cables and the networking interface of server and switches.

Table 1: Corresponding IEEE and IBTA electrical interfaces. Other combinations of signaling rate, number of lanes, and form factor exist (* The standards are still under development at this point in time).

FEC-aware active cable testing

With the advent of PAM4 modulation, a combination of digital equalizers and forward error correction (FEC) must be used to ensure error-free transmission. As a result, the complexity of measurements and test approaches has significantly increased compared to NRZ-based systems. Verifying the performance of transmitters now requires emulating a reference adaptive equalizer that accommodates the combined effects of the transmitter limitations and the transmission channel. Metrics such as vertical eye closure (VEC) and eye height (EH) are measured on a reconstructed eye (see Figure 4).

Figure 4: At 53 Gbaud, key metrics such as VEC and EH are measured on a reconstructed signal assuming a reference receiver with equalization capabilities.

When testing the performance of receivers, measuring the raw bit error ratio (BER) is not sufficient anymore at this data speed (-> White Paper: Forward Error Correction Challenges in 400G Device Test). Additional performance metrics are needed to qualify system performance:

Figure 5: Example of BER, FLR, and FEC margin measurement during stressed input tolerance test

Transmitter test

The transmitter test consists in characterizing the output of the module through the mated connector with a module compliance board (MCB). An oscilloscope is the main instrument for transmitter testing. It captures the signal and processes it by emulating the reference receiver described below.

Figure 6: IEEE 802.3ck reference receiver

This reference receiver includes:

EH and VEC are measured after the DFE. For more information about the transmitter characterization procedure, please refer to IEEE 802.3ck, Draft 3.2, Annex 120G.3.2.

Figure 7: Example of EH and VEC measurements on Keysight Infiniium equivalent-time sampling oscilloscope, using the eye-opening measurement method in annex 120G.5.2.

The values of EH and VEC are the values obtained after the reference receiver equalization. For this, the CTLE DC must be optimized together with the DFE taps. The values of eye height need to comply with the specification for EH (min 15 mV) where it also has a minimum value of VEC. This eye-opening measurement method is referenced from IEEE 802.3ck Draft 3.2, Annex 120G.5.2.
This measurement process can be done using Keysight’s electrical 802.3ck test app (D90103CKC or N1091CKCA). \

Figure 8: Auto-tune result of AEC, to find the optimal equalizer settings for near-end eye opening

Eye measurement will then use the optimal equalizer setting, to run the near-end EH and near-end VEC.

Figure 9: Example of measurement report of chip to module at TP4, with N1091CKCA Electrical IEEE802.3ck test app

Receiver test

The receiver test consists in testing the module interface with the worst allowable signal coming out of a host.
The receiver test setup consists of Keysight M8040A 64 Gbaud high-performance bit error ratio tester (BERT), a frequency-dependent attenuator or inter-symbol-interference (ISI) board, and a module compliance board (MCB). The pattern generator de-emphasis must be first optimized for the test channel and reference receiver (see section above). After this, its amplitude and jitter profile are tuned to meet the specified VEC and EH prior to performing the stressed input test. For more information about the stressed eye calibration, please refer to IEEE 802.3ck, Draft 3.2, clause 120G.3.4.

Figure 10: Stressed eye calibration results

The Stressed eye calibration results table shows the target EH and VEC to be achieved and the measured values after the CTLE optimization. Besides, the table also indicates the actual amplitude and random jitter (RJ) values to achieve the stressed input test calibration targets.

Keysight Active Cable Test Solution

Below is a complete setup for active time-domain (ATD) testing of active cables. It consists of M8040A bit error ratio tester (BERT), M8195A arbitrary waveform generator (AWG), ISI board, DCA sampling scope (N1000A DCA-X mainframe & N1060A precision waveform analyzer), test software (M8070B, N1010A, M8091CKPA & N1091CKCA) & accessories (cables, adapters, etc.)

Figure 12: Setup for ATD testing of active cables

The ATD method of testing contemporary high-performance data center interconnects as illustrated in this post, is undergoing review by the IBTA as an effective and more relevant form of a comprehensive test than those methods that preceded this FLR-based ATD technique. A summary of key benefits of this configuration are as follows:

limit
3