Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Industry Insights
Related Tags
- #Critical Communications
- #Customer Privacy
- #Wireless Device Test
- #Public Safety
- #Network Visibility
- #Energy Ecosystem
- #Test as a Service
- #BERT
- #PathWave
- #Network Test
- #Design + Automation
- #Communications
- #Autonomous Driving
- #SDN + NFV
- #Optical + Photonic
- #Lightwave Component Analyzers
- #Services
- #Arbitrary Waveform Generators
- #DDR5
- #GDPR
- #Oscilloscopes
- #Network Security
- #PCIe
- #Data Analytics
- #Education
- #PCIe 5.0
- #STEM
- #Environmental Sustainability
- #Semiconductor
- #KeysightCare
- #Healthcare
- #PAM4
- #Calibration
- #Cybersecurity
- #massive MIMO
- #Data Privacy
- #Design Software
- #mmWave
- #EMC Pre-Compliance
- #Data Center Infrastructure
- #Automotive + Energy
- #Manufacturing Test
- #Avionics
- #Automotive Ethernet
- #6G
- #Connected Car
- #Aerospace + Defense
- #Tunable Laser Sources
- #Gen 5
- #Network Analyzers
- #400GE
- #Sustainability
- #Signal Monitoring
- #In-Circuit Test Systems
- #EW
- #Internet of Things
- #Consulting Services
- #MilCom
- #Radiated Test
- #MIMO
- #5G
- #Blockchain
- © Keysight Technologies 2000–2021
- Privacy
- Terms
- Feedback
- Contact Us
Sheri DeTomasi
5G New Radio Solution Lead
Industry Insights
Understanding 5G New Radio Bandwidth Parts
2018-10-31 | 4 min read
A new concept in 5G New Radio (NR) is a feature known as bandwidth parts (BWPs). BWP enable more flexibility in how resources are assigned in a given carrier. Bandwidth parts are really about providing flexibility so that multiple, different signal types can be sent in a given bandwidth. Most base stations can utilize the wider bandwidths available in 5G. User equipment (UE) capabilities, however, will vary and it will be more challenging for some UEs to use the larger available bandwidths. Bandwidth parts enable multiplexing of different signals and signal types for better utilization and adaptation of spectrum and UE power.
LTE carriers are narrower in bandwidth, up to 20 MHz maximum that can be aggregated together to create a channel bandwidth up to 100 MHz in LTE-Advance, or up to 640 MHz in LTE-Advanced Pro. In comparison, 5G NR maximum carrier bandwidth is up to 100 MHz in frequency range 1 (FR1: 450 MHz to 6 GHz), or up to 400 MHz in frequency range 2 (FR2: 24.25 GHz to 52.6 GHz) that can be aggregated with a maximum bandwidth of 800 MHz.
With bandwidth parts, the carrier can be subdivided and used for different purposes. Each 5G NR BWP has its own numerology, meaning that each BWP can be configured differently with its own signal characteristic, enabling more efficient use of the spectrum and more efficient use of power. This feature is good for integrating signals with different requirements. One BWP may have reduced energy requirements, while another may support different functions or services, and yet another may provide coexistence with other systems. Bandwidth parts will support legacy 4G devices with new 5G devices on the same carrier. The following shows some examples of how bandwidth parts can support different services in a given carrier.
A bandwidth part is a subset of contiguous common physical resource blocks (PRBs). A UE can be configured with up to four BWPs in the uplink or four BWPs in the downlink. An additional four BWPs can be configured in a supplementary uplink. Only one BWP in the UL and one in the DL are active at a given time. This means the UE cannot transmit PUSCH or PUCCH and cannot receive PDSCH or PDCCH outside an active BWP.
This complicates how 5G NR signals are created and demodulated. BWP configuration parameters include numerology, frequency location, bandwidth size, and control resource set (CORESET). Now there are more test cases and permutations that need to be validated in 5G NR devices.
Learn more about 5G NR standards:
White Paper Series: First Steps in 5G: Overcoming New Radio Device Challenges Series and Webinar: Understanding 5G NR Physical Layer
Related Posts
RF + Microwave
IS YOUR SIGNAL ANALYZER UP TO TASK? PART 2: Three Advanced Noise Measurements to Expect from Your Modern Signal Analyzer
PARIS AKHSHI 2020.12.17
7 min read
#Signal Analyzers #Spectrum Analyzers #Measurement Fundamentals #5G
Industry Insights
Getting the Right Answer at the Right Time Keeps Projects on Track
Janet Smith 2020.12.14
3 min read
#KeysightCare #5G
RF + Microwave
IS YOUR SIGNAL ANALYZER UP TO TASK? PART 1: Three Advanced Power Measurements to Expect from Your Modern Signal Analyzer
PARIS AKHSHI 2020.12.11
6 min read
#Signal Analyzers #Spectrum Analyzers #Measurement Fundamentals #5G #Internet of Things