Enable browser cookies for improved site capabilities and performance.
Toggle Menu
Industries
Related Tags
- #Critical Communications
- #Customer Privacy
- #Wireless Device Test
- #Public Safety
- #Network Visibility
- #Energy Ecosystem
- #Test as a Service
- #Test Automation
- #Cloud Test
- #BERT
- #PathWave
- #Network Test
- #Design + Automation
- #Communications
- #Autonomous Driving
- #SDN + NFV
- #Optical + Photonic
- #Lightwave Component Analyzers
- #Services
- #Arbitrary Waveform Generators
- #DDR5
- #GDPR
- #Cloud
- #Clean Tech
- #Oscilloscopes
- #Performance Monitoring
- #Signal Analyzers
- #Data Analytics
- #Network Security
- #PCIe
- #Signal Generators
- #Education
- #PCIe 5.0
- #STEM
- #Software
- #Environmental Sustainability
- #Semiconductor
- #Industry Trends
- #KeysightCare
- #Healthcare
- #PAM4
- #Calibration
- #Cybersecurity
- #massive MIMO
- #Data Privacy
- #Design Software
- #mmWave
- #EMC Pre-Compliance
- #800G
- #Data Center Infrastructure
- #Automotive + Energy
- #System Calibration
- #Manufacturing Test
- #Avionics
- #Automotive Ethernet
- #6G
- #Power Supplies
- #Connected Car
- #Ethernet
- #Aerospace + Defense
- #Tunable Laser Sources
- #Gen 5
- #Network Analyzers
- #standards
- #400GE
- #Sustainability
- #Signal Monitoring
- #In-Circuit Test Systems
- #EW
- #Internet of Things
- #Consulting Services
- #MilCom
- #Jobs
- #Radiated Test
- #Post-Covid World
- #MIMO
- #5G
- #Blockchain
- © Keysight Technologies 2000–2023
Marie Hattar
Chief Marketing Officer
Industries
Happy together: solving the coexistence challenge for IoT devices
2018-09-07 | 8 min read
No one likes working in an overcrowded environment: it’s noisy, distracting, and interferes with what you’re trying to do. The same also applies to IoT devices. Ensuring reliable wireless performance in areas where there are many smart devices, all using different protocols on crowded radio bands, is challenging. These conditions often cause unexplained communications failures, even when the signal strength is sufficient for good operation.
These dropouts are often attributed to issues with coexistence, which is the ability of wireless equipment to operate in the presence of other devices using different communication protocols. The only way to ensure that devices deliver reliable wireless network performance, especially in mission-critical environments such as healthcare which demand uninterrupted connectivity, is to conduct rigorous coexistence testing. However, this is often easier said than done.
There are three main techniques which are commonly used to improve coexistence of devices and networks, but each has unique challenges that need to be overcome:
Physical separation: this aims to improve network operations by reducing the relative signal strength of two radio networks. By placing the two networks in different locations, each network experiences a weaker signal from the other, reducing the risk of interference. This can work well for some modulation types, but not all. For example, a hospital using the 2.4 GHz Industrial, Scientific and Medical (ISM) band may have thousands of wireless IoT devices using this band in operation, which makes physical separation impractical.
Frequency separation: this technique involves one network operating on a different frequency from another to reduce interference between the two, regardless of physical proximity. However, it is not always effective when it comes to the 2.4-GHz ISM band, which is occupied by overlapping Bluetooth, ZigBee, and 802.11 channels.
Time separation: here, transmissions are sent and received at different times to avoid collisions. However, as the volume of data transmitted on a network increases (which happens frequently in dynamic IoT ecosystems), simultaneous transmissions and collisions will occur more frequently. Additionally, most radio standards are not designed to detect other network transmissions and cooperatively share channels. This increases the chance of colliding transmissions that can cause errors and the need to retransmit data.
Designing your coexistence test
Despite these challenges, using one or more of these techniques is essential to enable reliable wireless performance for devices. This in turn requires an effective coexistence testing plan, which should include these four key stages:
First, you need to accurately model the environment for the device under test. This involves taking field measurements of the frequency band of interest, usually with a Real-Time Spectrum Analyzer, as it allows spectrum to be continually and accurately sampled with a high-speed analog to digital converter. A real-time fast Fourier transform can then be performed to convert the data into a spectral view and identify the types of signals present. Traditional swept-spectrum analyzers are often ineffective for this stage, as digital transmissions can come and go from the device before the sweep even reaches the frequency in use, which means it will not be detected.
After identifying the signals that are present, the type and number of signals needed to generate or model the coexistence test must be selected. This may mean choosing three different tiers of test signals, for example, one single Wi-Fi network passing data at the lowest tier, two Wi-Fi and one single Bluetooth signals at higher data rates, and then at the highest level, three Wi-Fi and five Bluetooth signals.
The next stage is to define the functional wireless performance of the device, by listing out its required functions. These may include device startup and connection to the wireless network (for example, in the healthcare facility), successful sending of status reports, regular data exchanges per minute while roaming between access points, and so on.
There are four possible ways to configure test equipment for coexistence testing. Each configuration uses similar components: the device under test (DUT), the device that connects or pairs with it, competing network devices, and a spectrum analyzer. The configuration to use depends on practical considerations, such as access to external antenna connections on the DUT, and whether the device has directional antennas. The options are:
When running coexistence tests and applying the results to your IoT environment, remember that these tests do not result in a simple ‘pass’ or ‘fail’. Rather, they focus on the probability that the device can meet its functional performance parameters in the test conditions. By varying those test conditions, device designers can chart the device’s coexistence behavior in detail, and mitigate the risk of interference affecting its performance in mission critical, real-world usage.
Find out more about how Keysight can help with IoT coexistence testing in our new white paper, and about our complete range of IoT test solutions here.
Related Content
Solutions
IoT Test Solutions
Related Posts
RF + Microwave
Cancer Patients Can Now Benefits from Smart Healthcare (IoT)
Paris Akhshi 2023.03.10
6 min read
#Healthcare #Internet of Things #Signal Analyzers #Spectrum Analyzers
Industries
Intelligent Software Test Automation: A Proven Roadmap for Business Success
Marie Hattar 2023.02.27
5 min read
#Industry Trends #Test Automation #Internet of Things #Performance Monitoring #Software
Simulation + Design
The Drive to Disrupt: How Digital Twins Are Fueling Automotive Innovation
Jenn Mullen 2023.02.23
12 min read
#Automotive + Energy #Autonomous Driving #Design + Automation #Design Software #Internet of Things #Industry Trends